AnsweredAssumed Answered

Can one add a user-defined calibration kit to a N9923A

Question asked by drkirkby on Oct 5, 2012
Latest reply on Oct 5, 2012 by drkirkby
I got my N9923A yesterday. I must admit I'm quite impressed with what such a small box can do. 

I noticed the N9923A supports several calibration kits, including the type-N 85032B that I have. I think it might also support my 3.5 mm calibration kit.  But is it possible to support a user-defined cal kit, where one enters the offsets is ps and capacitance coefficients C0, C1, C2 and C3? If so, where does one do this, as I can't seem to find it on the menus, though I've only "played" with it for an hour or so. 

I don't know my firmware version off-hand, but given it was shipped from Agilent only a week ago, I would expect it is up to date. 

The manual, at 139 pages, is a much lighter read than the documentation on my 8720D! 

Dave

Edited by: drkirkby on Oct 5, 2012 8:11 AM  

Outcomes