I found that there where changes since Vee 7 to now Vee 9 regarding the ID-files. Means: A file that is working in Vee 7 is now not compiling any more.
Sorry, I do not. I've never used the compiler myself. I just happened to have a copy of the manual.
There was something on the VRF this week:
" After removing all commands with: FOREGROUND (255,255,255),100; or BACKGROUND (230,220,210),0; ...I was able to recompile the file.
"
Why not compile it with the 7.0 compiler, and use the compiled version in your program instead of the uncompiled version as was also suggested on the VRF?
Attachments
I found that there where changes since Vee 7 to now Vee 9 regarding the ID-files.
Means: A file that is working in Vee 7 is now not compiling any more.
Do you have a change list for the compiler?
Sorry, I do not. I've never used the compiler myself. I just happened to have a copy of the manual.
There was something on the VRF this week:
Why not compile it with the 7.0 compiler, and use the compiled version in your program instead of the uncompiled version as was also suggested on the VRF?