AnsweredAssumed Answered

vrf Window size for a panel

Question asked by VRFuser on Sep 16, 2008
Latest reply on Sep 16, 2008 by VRFuser
"Schlieker, Reiner" <reiner.schlieker@siemens.com> wrote:
> VEE only has one window; all panels within VEE are displayed within
> this window.  You can set the window size and position with the
> geometry switch when running the program:
>
> -geometry widthXheight+/-xoffset+/-yoffset   e.g. -geometry 1024x768+0+0
> will size the window at 1024x768 and position it at the top left of
> the screen.
>
> Look in the VEE help under "command line options" for more info on this.
>

Or just execute    vee -?

and it will list all the available command line options.

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------


---
You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes