AnsweredAssumed Answered

vrf Urgent help!!

Question asked by VRFuser on Sep 16, 2008
Latest reply on Sep 16, 2008 by VRFuser
fdg Fgj <kolopipo@yahoo.com> wrote:
> Sorry for asking the same thing twice. Previously, I asked how to do
> resampling of a signal. The details are I am trying to convert come
> functions in matlab which is not available in VEE 8.5 student version.
> As we all know that Student version does not include matlab functions.
> I am trying to develop a program to do classification of ECG signals
> into some diseases like heart diseases. What I am doing is mainly
> signals processing.The first challenge I face is trying to resample
> the ECG signals received from a patient. The resampling process can be done easily using matlab function "resample".

             ^^^^^^^^^^^^^^^^^^^^^
>

>
> So I need help to convert the matlab functions like "resample" into VEE 8.5.
> Or is it impossible to do so? Are there anyways to convert the matlab
> functions so it can be used in the student version? I am only allowed
> to use student version.

umm --- checking Matlab docs shows that Build Arbitrary Waveform
        does the same thing as resample(ts,Time,'linear')

So the first one is easy. What's next?

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------


---
You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes