Hi,
Any idea how i can increase the max output source of 9310 to +30 dbm?
From the spec shows -127 to +13 dBm output level range (maximum +20 dBm settable), i need +30 dBm.
Adding amplifier at RF output will help?
Please advise.
Any idea how i can increase the max output source of 9310 to +30 dbm?
From the spec shows -127 to +13 dBm output level range (maximum +20 dBm settable), i need +30 dBm.
Adding amplifier at RF output will help?
Please advise.
Yes, the N9310A only supports up to +20 dBm power output. You may need the external amplifier. Please be careful of the possible reverse power in this case, which may cause damage to the RF front end of the signal source. DC blocker and RF isolator between the signal source and amplifier would be recommended based on your application.
I hope this was helpful -