AnsweredAssumed Answered

Triple Point of Water Using an SPRT, learn more...

Question asked by tomc on Sep 18, 2012
See how the triple point of water and other liquids are measured in a metrology lab. The triple point of water is defined as .01 degrees Celsius. At it's triple point water will exist as a liquid, a solid (ice) and a gas (vapor). In order to measure the temperature a Ponds Engineering K51 thermal electrically cooled core is used to lower the temperature below -8 degrees C. The core is then warmed to the triple point. A SPRT and an Agilent 34420A Micro-ohm meter is used to measure the temperature. The 34420A Micro-ohm meter has a low current mode which will reduce the measurement errors due to thermal warming. Watch this interesting video: http://www.youtube.com/watch?v=VyROvXPHx6s

For more information:
http://www.agilent.com/find/34420A  

Outcomes