AnsweredAssumed Answered

N5768

Question asked by mhj555 on Dec 16, 2011
Latest reply on Dec 20, 2011 by paulf
Is the N5768 power supply capable of sinking current?  I would like to use it in an application where there is another power source (perhaps another N5768) set to a fixed voltage, a load, and then the N5768 on the low side, regulating the current coming out of the load.
Is that possible to do?  If not, is there another power supply capable of doing that?

Thanks in advance for the help!  

Outcomes