AnsweredAssumed Answered

PSA E4445A with MXG N5182A ...

Question asked by kappasm on Sep 23, 2008
Latest reply on Sep 25, 2008 by kappasm
Hi,

I have pair of struments:

PSA E4445A + MXG N5182A with External Source Control Measurement Personality, Option 215.

I configured hardware as indicated by the PSA during the setup of the "Source Control". MXG is placed automatically in "Remote Control". Setup a simple sweep 500 MHz to 1000 MHz, but the PSA continues to see the background noise and not a line set at power out of generator. Touching on the PSA RBW (enlargement) starts to operate but not at the level set on the generator.

It is possible that there is some problem with software and / or setting ?

Thansk.

Kappasm.  

Outcomes