I realize there's a "Get File Name" under the System menu, but I'd like the program's file name.
Like if I'm running a file called example_42.vee, is there a function that returns "example_42" (or with the extension, I'm not picky).
Like if I'm running a file called example_42.vee, is there a function that returns "example_42" (or with the extension, I'm not picky).