I'm running VEE 9. I had a VEE application that failed in the middle of cmd'ing an instrument (811). then when i bring the application back up i get this error 814. I have only been having this problem since i switched to VEE9. thanks
I should have also mentioned that the big issue is that in order to clear the error i have to shut the computer down!! just shutting down the instrument and VEE doesn't do it.