AnsweredAssumed Answered

Can't connect to N5244A via LAN

Question asked by herbert on Sep 2, 2012
Latest reply on Sep 4, 2012 by herbert
I have been plowing through all the docs and can't seem to find an answer.  It feels like I am missing something obvious.  I am trying to connect to the N5244A over a LAN and have no success.  I can ping the device but when I try using NI Measurement & Automation explorer or  the Agilent IO Control to add the N5244A I do not get a connection to the device.  It is not found.  Yet I can add other instruments.

  I would like to do some LabVIEW programming, using the Agilent drivers, but cannot get past first base.  I cannot open a VISA session in NI MAX or Agilent IO Control.  I am suspecting there is a configuration problem on the N5244A.  Any suggestions you might have would help alleviate some frustration!  Thanks.  

Outcomes