AnsweredAssumed Answered

How to set current directory.

Question asked by virgiltu on Mar 9, 2011
Latest reply on Mar 10, 2011 by Woozie
I am looking of a way to have the program pull files from the current directory in with is located it.

So far i have to set up a variable with a constant like .//veefiles/       then i can call this variable all over the program. However if i move the folder veefiles to the desktop now i have to go and set the variable to the new location. Is there any way to set up the program to pull files from the current directory. I know for example unless specified in PHP i can just use    /file.vxe and the files will run from the directory. If i need to go down one lever i will go something like  ./file.vxe or to root ../file.vxe   . As i said this is a php example, is there something similar in VEE?


Thank you  

Outcomes