AnsweredAssumed Answered

8510C Warning: IF CaFailed on test channel

Question asked by LynnChidester on Mar 28, 2008
In checking out a university 8510 (upgraded to CRT C version), I get (on doing a self test, test 22) IF Cal Failed on test channel.  The service manual instructs to troubleshoot the problem (85102) using 85102-60210 adapter.  As is often the case, said adapter is nowhere to be found.  While the adapter can be purchased from Agilent (~$4500), I'm hoping for a less costly option to continue the 8510 checkout.

Can anyone provide other less expensive options (like information on which connections to make from the BNC to the other coaxial connections?  

Outcomes