AnsweredAssumed Answered

Synchronizing Multiple Agilent Function Generators, As an example a 33220A

Question asked by lhornburg Employee on Sep 17, 2012
Latest reply on Oct 9, 2012 by lhornburg
Watch this video: Synchronizing multiple Agilent Function Generators. See how-to phase lock an Agilent 33220A Function Generator with a 33250A Function Generator. A second cable BNC cable is needed but not shown in the video. The second BNC is used to connect the "Master" Trig Out to the "Slave" Trig In. http://www.youtube.com/watch?v=r1SwXRns_qs

For more information: http://www.agilent.com/find/33220A  

Outcomes