AnsweredAssumed Answered

Is there any chance an N9923A could be used down to 1.75 MHz?

Question asked by drkirkby on Sep 1, 2012
Latest reply on Sep 6, 2012 by am95405
I know the lower frequency limit of the N9923A is 2,0 MHz, but I wonder if there's any chance a future firmware upgrade could permit it the lower frequency limit could be changed to 1.75 MHz, even if the accuracy is compromised? 

I'll be perfectly honest, my reason for wanting this is to cover the 1.8 to 2.0 MHz (160m) amateur band. As a ham owning a N9923A, it would be nice if it could be used on the lowest HF amateur band. 

Hopefully any such firmware upgrade would not be an expensive option! Or perhaps there are reasons it will never be possible to get below 2.0 MHz. 

Dave (G8WRB)  

Outcomes