AnsweredAssumed Answered

GPIB/LAN Gateway indicates max connected devices.

Question asked by vanbuba on Jan 10, 2011
Latest reply on Jan 19, 2011 by vanbuba
(I'm not sure where to post this.)
Company: Northrop Grumman Electronic Systems

When connecting to the E5810 via the web interface, The SICL address list is filled, meaning gpib0,1 through gpib0,31 (not gpib0,21 this is the E5810). I have no cables hooked up to the device. Agilent IO Libraries 1.6 allows connection to the devices but fails the '*IDN? command (obviously). Interestingly, I have recently connected a NI Instrument Simulator to the serial port of the gateway and all works well.

Has anyone seen this problem before? Is it firmware, settings, etc? I use, maintain/program via, dozens of these products and never had any issue.

Thank you,
Barry  

Outcomes