Hi there,
I had installed the Intuilink v1.1 for the PNA E8362B. My problem is my PC can't connect to the PNA. Is it I need to connect both PC and the PNA with LAN first and then try to run the Intuilink ? I tried to configure the GPIB address that I used. I had installed the IO Library Suite. The IO library suite can detect the PNA. Its adress is GPIB0. So how should I write the address at the Intuilink ? Is it I need to install the Intuilink in the PNA ? Thanks
Regards,
Dayah
I had installed the Intuilink v1.1 for the PNA E8362B. My problem is my PC can't connect to the PNA. Is it I need to connect both PC and the PNA with LAN first and then try to run the Intuilink ? I tried to configure the GPIB address that I used. I had installed the IO Library Suite. The IO library suite can detect the PNA. Its adress is GPIB0. So how should I write the address at the Intuilink ? Is it I need to install the Intuilink in the PNA ? Thanks
Regards,
Dayah
Last Intuilink for PNA (& Helper File):
http://www.home.agilent.com/agilent/edi ... 1:epsg:sud