I found it using the handy-dandy "Home/Programming" in PNA help where it has:
Programming Guide
_____
Two ways to find programming commands:
1.
From a simulated PNA User Interface
New
mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/XComFinderSet.htm
Legacy
mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/CommandFinderSet.htm
GPIB / SCPI
COM
2.
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GP-IB_Command_Finder/SCPI_Command_Tree.htm"Command Tree
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/COM_Reference/Objects/The_Analyzer_Object_Model.htm"COM Object Model
See Also
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GPIB_Example_Programs/SCPI_Example_Programs.htm"Example Programs
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/COM_Example_Programs/COM_Example_Intro.htm"Example Programs
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/Learning_about_GPIB/Learning_about_GPIB.htm"Learning about GPIB
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/Learning_about_COM/Learning_about_COM.htm"Learning about COM
And I use the "From a Simulated PNA user interface" to find the commands related to a pulldown, which are:
CALCulate<cnum>:MARKer<mkr>:SET <char>
(Write-only) Sets the selected instrument setting to assume the value of the specified marker.
Marker Functions CENT, SPAN, STARt, and STOP do not work with channels that are in HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/S1_Settings/Sweep.htm#SweepTypeDiag"CW or HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/S1_Settings/Sweep.htm#segment"Segment Sweep mode.
HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GP-IB_Command_Finder/Calculate/Marker.htm#Critical"See Critical Note
Parameters
<cnum>
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.
<mkr>
Any marker number from 1 to 10; if unspecified, value is set to 1
<char>
Choose from:
CENTer - changes center frequency to the value of the marker
SPAN - changes the sweep span to the span that is defined by the delta marker and the marker that it references. Unavailable if there is no delta marker.
STARt - changes the start frequency to the value of the marker
STOP - changes the stop frequency to the value of the marker
RLEVel - changes the reference level to the value of the marker
DELay - changes the line length at the receiver input to the phase slope at the active marker stimulus position.
Examples
CALC:MARK:SET CENT
calculate2:marker8:set span
Query Syntax
Not Applicable
HYPERLINK "javascript:hhctrl.TextPopup(DefSCPI,'Arial,8',10,10,00000000,0xc0ffff)"Default
Not Applicable
_____
_____
From: Walker, Richard [mailto:Richard.Walker@Herley.Com]
Sent: Monday, May 12, 2008 8:41 AM
To: PDL-LISTS,VRF (A-Lists,unix1)
Subject: [vrf] vrf - IEEE command for PNA - Marker > Delay?
Vee users,
Can someone point me in the correct direction for the IEEE command (Marker to Delay)?
Thanks
Richard A. Walker
RF Automation Specialist, LLC
Cell: (631) 834-6293
_____
The information contained in this message may be confidential and legally privileged. If you are not the intended recipient of this email and its attachments, you must take no action based upon them, nor must you copy or show them to anyone.
Please contact the sender if you believe you have received this email in error.
---
You are currently subscribed to vrf as: joel_dunsmore@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".
---
You are currently subscribed to vrf as: ming_meng@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".