AnsweredAssumed Answered

Testing ABS With An N6705 DC Power Analyzer, and a DUT with Dynamic Power

Question asked by paulf on Sep 10, 2012
The N6705 DC Power Analyzer is used to simulate intermittent DC Power to an ABS module. The ABS module was originally not designed to handle the intermittent voltage. The engineers were able to simulate the intermittent voltage and design a Anti-lock Braking System module that can handle the voltage drop out.

The N6705 was ideal for the task as it combines a DC power supply with an arbitrary waveform generator.

Watch video: https://www.youtube.com/watch?v=5zOMZy9kus8

For more information: http://www.agilent.com/find/n6705  

Outcomes