AnsweredAssumed Answered

Virtual Panel for U2000A USB Power sensor in VEE

Question asked by steveor on Jun 19, 2012
Latest reply on Jun 28, 2013 by matthew_rose
Hi,

I visited the agilent web site:
[http://www.home.agilent.com/sec/techSupport.jspx?pid=1079918&pageMode=DS&cc=US&lc=eng&pselect=SR.PM-Search%20Results.Drivers,%20Updates%20%26%20Examples] 
And downloaded the virtual panel for the U2000A USB power sensor.  This nice utility allows me to communicate with my USB power sensor.  The only problem is, the virtual panel is offered as a secure runtime version (.vxe).  It would be quite helpful to have the source code for this example.  Can I get the .vee version?  Without this, the utility only shows it is POSSIBLE to communicate with the sensor, but it would be much better to have the source code so I can follow this example in detail.  Then, I could modify the code and use this in my application.

Thanks,
Steve Ortiz

Outcomes