Hi,
I need to have an FM input signal for my circuit. The 33220A signal generator is capable of generating an internal FM signal with maximum 20KHzmodulating signal. So i am using two 33220A signal generators one's output is connected to another's Modulation In connector in the back. In the user manual (http://cp.literature.agilent.com/litweb/pdf/33220-90002.pdf) page 85
it is written that :
"If you select the External source, the carrier waveform is modulated
with an external waveform. The frequency deviation is controlled by
the ±5V signal level present on the rear-panel Modulation In
connector. For example, if you have set the deviation to 100 kHz,
then a +5V signal level corresponds to a 100 kHz increase in frequency.
Lower external signal levels produce less deviation and negative
signal levels reduce the frequency below the carrier frequency.".
For an FM signal assuming frequency deviation Df=kf * Am where kf is sensitivity Hz/V and Am is the modulating signal amplitude; does it mean that for an FM signal with Df=100KHz i need to give Am=10Vpk-pk= 5V in amplitude? Does kf=20KHz/V ? If i apply Df=100KHz from the first signal generator (in which i set carrier frequency and external FM option) and Am=2Vpk-pk=1V in amplitude sine wave from the signal generator will i end up with Df=20KHz ?
Thanks
HIDIR ASKAR
Edited by: HIDIR on Feb 14, 2013 4:19 PM
I need to have an FM input signal for my circuit. The 33220A signal generator is capable of generating an internal FM signal with maximum 20KHzmodulating signal. So i am using two 33220A signal generators one's output is connected to another's Modulation In connector in the back. In the user manual (http://cp.literature.agilent.com/litweb/pdf/33220-90002.pdf) page 85
it is written that :
"If you select the External source, the carrier waveform is modulated
with an external waveform. The frequency deviation is controlled by
the ±5V signal level present on the rear-panel Modulation In
connector. For example, if you have set the deviation to 100 kHz,
then a +5V signal level corresponds to a 100 kHz increase in frequency.
Lower external signal levels produce less deviation and negative
signal levels reduce the frequency below the carrier frequency.".
For an FM signal assuming frequency deviation Df=kf * Am where kf is sensitivity Hz/V and Am is the modulating signal amplitude; does it mean that for an FM signal with Df=100KHz i need to give Am=10Vpk-pk= 5V in amplitude? Does kf=20KHz/V ? If i apply Df=100KHz from the first signal generator (in which i set carrier frequency and external FM option) and Am=2Vpk-pk=1V in amplitude sine wave from the signal generator will i end up with Df=20KHz ?
Thanks
HIDIR ASKAR
Edited by: HIDIR on Feb 14, 2013 4:19 PM
If I want to have 80KHz frequency deviation for my FM signal according to my first thread i try three solutions;
1) Apply 100KHz from the 1st signal generator for frequency deviation variable and choose Am=8Vpk-pk=+/-4V amplitude from the second signal generator as the modulating signal amplitude (since Df=Am*kf, here kf=20KHz ?).
2) Apply 80KHz from the 1st signal generator for frequency deviation variable and choose Am=8Vpk-pk=+/-4V amplitude from the second signal generator as the modulating signal amplitude.
3) Apply 80KHz from the 1st signal generator for frequency deviation variable and choose Am=10Vpk-pk=+/-4V amplitude from the second signal generator as the modulating signal amplitude.
If one of them is right I should have the same using 20*log10(J1/J2)=J1inDB_fromFFT - J2inDB_fromFFT where J1 and J2 can be found from Bessel function table attached. But it is not always correct when I look at J1 and J2 in DB from oscilloscope FFT views aattached for conditions 1,2 and 3; where modulating signal fm=40KHz sine and carrier amplitude is 2Vpk-pk sine wave are applied.
The modulating index should be Df/fm=80/40=2 and from the table J1=0.58, J2=0.35 so 20*log10(58/35)= 4.3872 dB.
For the 1st condition (attached figure 1.bmp) J1inDB_fromFFT - J2inDB_fromFFT=6.95-1.75 = 5.2 dB
For the 2nd condition (attached figure 1.bmp) J1inDB_fromFFT - J2inDB_fromFFT=9.75-1.75 = 8.0 dB
For the 3rd condition (attached figure 1.bmp) J1inDB_fromFFT - J2inDB_fromFFT=8.75-1.75 = 7.0 dB
It seems that the first is right but i am not sure.
What should I do to choose a specific frequency deviation ? Any comment or help please.
HIDIR