AnsweredAssumed Answered

PNA-X Firmware maker frequency setting issue for 'MHz' bug report

Question asked by rok on Jan 2, 2013
Latest reply on Jan 3, 2013 by daras
Hello,

I am using A.09.80.15 firmware and am trying to set a marker for an SMC channel I am configuring in the Megahertz units.  If I try to type in the value (i.e. 200 MHz) and use a lowercase 'm', it will not set it.  Only if I use an uppercase 'M' does it set it to the right frequency value for the marker. I tried the same experiment for the Gigahertz units (i.e. 1GHz) and it worked regardless of whether a lowercase or uppercase 'G' was used or not. At first, I thought it was a marker setting issue until I tried out the uppercase 'M'. Just wanted to report the bug in case someone else encountered that same problem.

Best regards,
rok  

Outcomes