AnsweredAssumed Answered

Is it compatiable NI GPIB-USB-HS with agilent 34970A Data Acquisition?

Question asked by pak on Jul 30, 2012
Latest reply on Jul 30, 2012 by pak
Hello dude,
     I'm a new to agilent product. I have 34970A Data Acquisition / Data Logger Switch Unit which is intended to used for data logging. And I have a NI GPIB-USB-HS GPIB controller (http://sine.ni.com/psp/app/doc/p/id/psp-354/lang/en) which is used for communication between PC and 34970a. The system info of PC is Windows XP SP3. My setup for these devices are as follow:
1) Install NI driver for NI GPIB-USB-HS
2) Install Agilent IO Libraries Suite 16.2
3) Install BenchLink Data Logger 3 Software for 34970A/34972A

After installing, NI can detect NI GPIB-USB-HS, but Agilent IO connection expert cannot. So my question is, Is it 34970A compatible with NI GPIB-USB-HS GPIB controller? If answer is yes, please guide me how to solve the communication problem.

Best regards,
pak  

Outcomes