AnsweredAssumed Answered

Can we have 7 step calbration macro on old PNA-L N5230A

Question asked by mirek on Jan 2, 2013
Latest reply on Jan 3, 2013 by Dr_joel
The old PNA-L (N5230A 1.1Ghz CPU) do not support the short calibration (7 step cal for four ports) method. I do not expect that the firmware (A.07.50.67) will be updated as the unit is out of production for several years. I just wonder if Agilent could prepare calibration macro that could run on old PNA-L that will support seven steps manual calibration. 

The existing manual calibration method is very long.  

Outcomes