Hey everybody,
I am trying to toggle an output digital signal with the data acquisition device USB-6501 using Agilent VEE Pro 9.2.
I was able to communicate with the device without any problem, and I am also able to use the action commands.
However, when I looked into the manual, it stated that the input required by the "write digital output" required an UINT8 input (since the device has 8 lines per port);
but when I look into the command options, it stated that it'll only read UINT16 inputs...
I tried to use both, however neither seem to work.
When I tried to input "true" or "1" into P0.0, the value that I read on the DMM is still almost zero (instead of the 4.7 V I was expecting).
If anyone can please let me know if I am doing something wrong, I would highly appreciate it!
Phantom
I am trying to toggle an output digital signal with the data acquisition device USB-6501 using Agilent VEE Pro 9.2.
I was able to communicate with the device without any problem, and I am also able to use the action commands.
However, when I looked into the manual, it stated that the input required by the "write digital output" required an UINT8 input (since the device has 8 lines per port);
but when I look into the command options, it stated that it'll only read UINT16 inputs...
I tried to use both, however neither seem to work.
When I tried to input "true" or "1" into P0.0, the value that I read on the DMM is still almost zero (instead of the 4.7 V I was expecting).
If anyone can please let me know if I am doing something wrong, I would highly appreciate it!
Phantom