AnsweredAssumed Answered

ADS 2009 momentum WARNING

Question asked by jon on Dec 19, 2012
Latest reply on Dec 30, 2012 by neptune
Hi users, 

I am facing a momentum warning and I am not able to solve the issue. 
The warning says :

WARNING : For one or more occurrences of a via incident to
an empty part of a STRIP layer, covering the via
by an autogenerated shape on the STRIP layer was
rejected. This happens when none of the masks
mapped to the STRIP layer has the same material
definition as the VIA mask. Please cover these
vias manually or provide a mask with the same
material definition as the via. Further details
have been written to the DRC report.

Could you help me to understand the meaning of it? All vias are defined in the substrate definition.

thanks  

Outcomes