AnsweredAssumed Answered

HP 70K tracking generator 70300A

Question asked by on4wx on Jul 27, 2012
Latest reply on Jul 27, 2012 by tabbott
Hi All,

I have a 70k System with the following configuration:

70206A System Graphic Display

70900A: Rev 880901
70902A: Rev 871027
70908A: Rev 870721
70300A: Rev 870910


 
I would like to have the capability to sweep the frequency with the tracking generator using a frequency multiplier but when I activate the tracking generator, the spectrum unit doesn't measure above 2.9 ghz.

Is it possible to perform this measurement by disengaging the control of RF Section by the sweep generator ? I don't find any option in the menu ?


Thanks a lot for your support.

Kind Regards / Best 73's


Stephan ON4WX  

Outcomes