AnsweredAssumed Answered

reading trace data for droop calculations on N1911A

Question asked by nsm on May 30, 2012
Latest reply on Jun 28, 2013 by matthew_rose
Hi,

I using an N1911A for doing pulsed measurements. I want to read the trace data for droop calculations. I am using the following sequence to read the data. Is it necessary to use the Fetch? command.If I use the fetch command, how can I figure out if the operation has completed? If I send an *OPC?  when the fetch read operation is being performed,i get an error command saying that the query is unterminated. Can somebody help me on this?

TRIG:SOUR INT
INIT:CONT OFF
TRAC:STAT ON
INIT
FETCH?
TRACE:DATA? LRES


Rgds

Outcomes