I switched to Vee 9.2 on a Windows 7 64bit system.I used to work on Vee 9.0 on a Windows XP system where I created a lot of programs.
Now on Vee 9.2 the MATlab script of my old programs doesn't work anymore showing the following error messages:
Error 591: Could not start MATLAB Engine
and after another try
Error 592: Workspace Initialization failed
What can I do to solve this problem?
Now on Vee 9.2 the MATlab script of my old programs doesn't work anymore showing the following error messages:
Error 591: Could not start MATLAB Engine
and after another try
Error 592: Workspace Initialization failed
What can I do to solve this problem?
When using Agilent VEE 9.2 in Windows 7 64-bit using WOW64 emulator, please be informed of the following limitations:
1. Error running Agilent VEE runtime programs containing Matlab scripts
If you are running Agilent VEE runtime programs (.vxe) containing Matlab scripts for the first time, the error dialog "Matlab engine could not be started" might appear. Steps to fix this:
Go to Start | Run and type 'secpol.msc'.
In the prompted dialog, navigate to Local Policies | Security options.
Set the value of User Account Control: Run all administrators in Admin Approval Mode to Disabled.
Run the Agilent VEE runtime program again and it should work fine.
After that, you may re-enable Run all administrators in Admin Approval Mode and the Agilent VEE runtime program should still run well.