AnsweredAssumed Answered

E4443A Analyzer default settings?

Question asked by Tehrasha on Apr 14, 2008
Latest reply on Apr 28, 2008 by jborges3
Our analyzer appears to randomly loose various settings between power cycles.

Most days it comes up in exactly the same state it was shutdown in, but sometimes the GPIB bus address is wrong, or it forgets that it was set to use an external standard.  Quite often it sets the PowerOn/Preset to a non existant 'user preset' that tries to compesate for an external amplifier, which even a 'Factory Preset' will not clear.  I have to go in and remove the compensation manually.

It would not be so bad if it -consistantly- came up with differnet settings, but its so sporatic that it is quite annoying.

Is there something I am missing?  

Outcomes