AnsweredAssumed Answered

I believe there's an error in the 85055A 'N' verification kit manual

Question asked by drkirkby on Jan 13, 2013
Latest reply on Jun 22, 2013 by drkirkby
If I'm not mistaken, there's an error in the manual for the 85055A 'N' verification kit. 

http://cp.literature.agilent.com/litweb/pdf/85055-90014.pdf

Given this is a current model, if I'm right, Agilent should probably correct it. 

Figure 2-1, page 2-3, shows a male and female N connector. The pin depth of the male is shown as 5.26 mm (0.207") *maximum*. I believe it should be a *minimum* of this, not a maximum. If the depth is any less, the male and the female will damage each other. 

I'm guessing here is as good as any place to report such an error. 

Dave

Edited by: drkirkby on Jan 13, 2013 12:04 PM  

Outcomes