Hello, I am trying select the service menu but the password given in the service manaul does not work, is there anyway to change this password or send it back to MFR default? I don't want to have to do an entire wipe and reinstall software if I don't have too.
Make sure you are pressing: [Service], [-], then the two digit code from the service guide, then [Enter]. Don't forget the minus sign.
Now pressing the [Service] softkey again should display the service softkey menu, where you can (for example) toggle the Flatness data on/off, or the Band Lock.
This password cannot be changed by the user.
You should be aware of the following features that do not require access to the service menu:
If you want to reset system defaults, press: [System], [More 1 of 3], [Restore Sys Defaults].
If you want to reset the alignment default data, press: [System], [Alignments], [Restore Align Defaults].
I hope this helps.
What is the underlying problem you are seeing that is prompting you to use the diagnostic features ?
Regards, Simon C.