AnsweredAssumed Answered

U1051 Measurement Duration

Question asked by natant on Dec 19, 2012
The following is quoted from the user manual of the 1050A & U1051A (page 17):

"The nominal range limitation of 10.48 ms can be completely removed if a channel can be dedicated to the measurement of a known repetitive pulse. A square wave with a period just under 200 Hz would be appropriate."

Why is the specific frequency of 200 Hz mentioned?  I have a square wave of 10kHz, duty cycle 50%.  Will that also work?  

Outcomes