AnsweredAssumed Answered

Using VEE to control Voltec 1000+

Question asked by andrwong on Apr 20, 2010
Hi,

I'm new in VEE, practically a newbie. I'm having problem to control Voltec 1000 by using VEE. As the instrument can be detected in VEE by using direct I/O, i assume it can be controlled. However, when i wrote simple program "IDN?" it prompt up an error 811 which is a timeout error. After that, the instrument can't be detected anymore and i need to use Agilent I/O Expert to refresh the connection and not refresh using VEE. Pls help to advise if anyone encounter this issue before.In short, i need to do some programs to control the Voltec 1000+
BTW, Voltec 1000+ does support SCPI command.

TQVM.  

Outcomes