Answer: The ESG/PSG power level is distributed equally among the satellites. In the case where there are 8 satellites and an ESG total output power of P(esg) in dBm, with all satellites being equal power, the power of an individual satellite would be P(esg) – 9dB. So, if you have ESG set at -80 dBm, then each satellite is at -89 dBm