*FAQs for N7609B-EFP Basic Single Satellite Waveform Mode*
Question: I need to use the same set of waveform files on multiple test stations. Is there some way to transfer them to each signal generator without having to connect the N7609B software to each instrument and download individual waveforms?
Question: I need to use the same set of waveform files on multiple test stations. Is there some way to transfer them to each signal generator without having to connect the N7609B software to each instrument and download individual waveforms?