AnsweredAssumed Answered

Any tips to adjust VNA setting when looking at highly reflective devices?

Question asked by drkirkby on Jan 6, 2013
I'm trying to measure some devices which are basically open and short circuits, so |rho| is close to 1.0, or a reflection coefficient of close to 0 dB. 

Is there anything I can adjust on the VNA to improve accuracy of such measurements? I'm particularly keen to know the capacitance of an open as accuratly as possible. 

I was thinking of perhaps reducing the source power, so the amplifiers are operating in a more linear region. Is a full 2-port calibration necessary or reccomended when looking at these sort of devices? 

I assume my question is pretty general, and would apply to any VNA, but if there is something specific to certain models, mine is an 8720D. 

Dave

Edited by: drkirkby on Jan 6, 2013 5:08 PM  

Outcomes