AnsweredAssumed Answered

pna-x how to save .s2p &.s2px for smc channels using scpi

Question asked by rok on Nov 2, 2012
Latest reply on Nov 6, 2012 by daras
Hello,

I'm using the latest firmware of A.09.80.03. I'm trying to save the .s2p and .s2px files for my smc gain measurement channel. I'm able to do it manually using the 'Save Data As' command from the 'File' menu. I'm trying to figure out how to do it under SCPI. In looking thru the help file, it directed me to the "Calculate:Data Commands" section. However, the listed commands stated that it will only work on S-Parameter type measurements only. I did try the following:

CALC5:PAR:MNUM 5
CALC5:DATA:SNP:PORTS:SAVE '1,2','C:\TEMP\TEST.S2P';*OPC?

but I get a Error 106, measurement not found error. In the example above, I have Tr#=5 and it is residing under channel 5. So I'm thinking the commands didn't work since I was in an SMC channel and not the standard S-parameter channel. Can someone list the way to save both a .s2p and .s2px files using SCPI on an SMC type measurement channel?

Thanks,
rok  

Outcomes