I am using my company's Agilent N5306A logic analyzer for the first time. There are two blades in the N5541A-N2X chassis. I'd need to synchronize the timing of two PCIe probes from this box. Assuming that I can only have one probe on each blade, what do I need to synchronize the timing of the two blades? Are the blades already connected by virtue of being in the same chassis, or do we have to purchase a separate cable for the "TIMING SYNC" ports on the back of the blade?
Also, do I need an extra piece of equipment to act as the master clock, or is cabling the two blades together enough?
Thanks!
Tom
Also, do I need an extra piece of equipment to act as the master clock, or is cabling the two blades together enough?
Thanks!
Tom