AnsweredAssumed Answered

AUX IF OUTPUT

Question asked by SOLT_guy on Dec 23, 2012
Latest reply on Mar 25, 2013 by tabbott
Dear Sir:

       I own a 8593E SA.   On the back of the SA, there is BNC connector for the AUX IF output (21.4 MHz).

      I am led to believe that this output can be used to demodulate an incoming RFsignal?  

      Can you please reply and tell me whether this output can be used for this application and the appropriate demodulating circuit type (if the output signal type is fixed)  that should follow this stage?

      However, I have option 130 (narrow bandwith installed)  and when an option is installed some signal re-routing within the SA is done.    

      Can you please reply and tell me if this output can be be used for demodulation purposes if option 130 is installed?

      Please take notice that these are two separate questions that require separate answers.    Your feedback would be appreciated.

Edited by: SOLT_guy on Dec 24, 2012 12:26 AM  

Outcomes