AnsweredAssumed Answered

N9923A SCPI commands don't function as expected

Question asked by eagleeye1210 on Jan 28, 2013
Latest reply on Jan 29, 2013 by am95405
Recently I'm working on controlling FieldFox using SCPI commands, and I find that  two SCPI commands don't work as expected.
1. :SENS:CORR:USER?
      If I only calibrate port 1 of FieldFox, when the active measurement is S22, I expect that :SENS:CORR:USER? will return "0" as PNA does, but actually this command returns "1".

2. CORR:COLL:METH:TYPE?
     This command always returns SOLT1, no matter what calibration I have done using the control panel of the FieldFox.
I'm using N9923A, and firmware release is A.06.15.
Is there anyone who could help me out? I really need these two functions work as expected.  

Outcomes