AnsweredAssumed Answered

The 85033E 3.5 m cal kit has no sliding load. So why offer it during cal?

Question asked by drkirkby on Sep 18, 2012
Latest reply on Sep 18, 2012 by dhamilton
I've got an 8720D VNA (latest firmware), which has support in the firmware for the 85033E 3.5 mm calibration kit. 

I'm puzzled why there are options for lowband, broadband and sliding loads, when there is only one load in the kit, and that is not a sliding load. 

Dave  

Outcomes