AnsweredAssumed Answered

N9310A sweep duration

Question asked by WiktoriaJ on Dec 1, 2011
Latest reply on Dec 2, 2011 by WiktoriaJ
Hello,
I've noticed something peculiar while using my N9310A generator to generate RF sweeps: overall time of sweep is longer than the number of steps multiplied by their dwell. When I set it to generate 200 steps with dwell of 10 ms, the sweep is approximately 11 s long.
Is that supposed to happen or is there something wrong with my generator?
If this situation is normal, how can I calculate the duration of my sweep?
Thanks for the answer in advance
Wiktoria  

Outcomes