Hello,
I'm going to use N8731A power supply with superconductive load, so the load resistance is almost zero and the load inductance is relatively high (0.01 - 3 mH). Are there any recommendation regarding additional equipment (filters, additional resistors etc.) which I might need?
Thanks in advance,
Mikhail
I'm going to use N8731A power supply with superconductive load, so the load resistance is almost zero and the load inductance is relatively high (0.01 - 3 mH). Are there any recommendation regarding additional equipment (filters, additional resistors etc.) which I might need?
Thanks in advance,
Mikhail
What level of current will be required by the inductance?
How do you anticipate bringing the L on and off line?
The N8731A will likely not have the current sinking ability to bring down the L. Answers to the previous questions will aid in recommendations.
Regards,
PeterW