AnsweredAssumed Answered

Intermit sweeps

Question asked by hlodwig on Jan 4, 2013
Latest reply on Jan 21, 2013 by hlodwig
Hello,

I use a 8164B Mainframe with a 81600B - 201 TLS, driven by the PFL in my software.

This system is designed to sweep continuously, except when the TLS need a lambda zeroing. But sometimes, it stops the sweeps during around two minutes, without error or explanation message. I guess that's not a lambda zeroing, because it's too fast.

So what are theses pauses in the sweeps ? It is normal ? It is in cause of the PFL ?

Thanks in advance.  

Outcomes