I'm looking to run some type of program or script (I've never done any programming, so take whatever I write with a grain of salt) that can turn the RF on for 30 minutes and and then off for 4 hours and loop it. I'd have the signal generator connected directly to a laptop that will be there full time; it is in a room without internet access. The machine is well ventilated and can be left on at all times with all of the proper settings, I just only want signal output for 30 minutes every 4 hours. Can you please provide me either with the script I'd need to run and instructions on how to run it or whatever information/manuals someone computer savvy would need to write this program himself would need?
I'm happy to provide more info if its needed. Thanks in advance!
I'm happy to provide more info if its needed. Thanks in advance!
Attached is a C-sharp program zipped up. We have added a note for making modifications. The timing is set for 30min on and 4hrs off.
Enjoy!