AnsweredAssumed Answered

Oscillator pin layout.

Question asked by fcss on Nov 4, 2010
Latest reply on May 5, 2011 by tabbott
Hello. I have an HP 5086-7366 YIG oscillator (serial No. 01604) and would like to get the schematics and pin layout of the RF module ,i.e., the bulky part where the YIG sphere is encapsulated. The module has 10 pins and is connected to a small circuit board with the following reference numbers in it (A-2320-53 and 5061-5418). The schematics of that board are also welcome. I have looked around and have not found much on it. Thanks in advance. Fabio.  

Outcomes