AnsweredAssumed Answered

Fundamental question about Agilent network analyzer (E5071A)

Question asked by wangyiliu99 on Feb 20, 2013
Latest reply on Feb 21, 2013 by Dr_joel
Hi, all

The advantest network analyzer(NA) is being used, however, we are considering switch to agilent NA.

cost and sweep time are the main concerns.

Here are the questions
(1) in the sweep mode, there are stepped, swept, high speed swept.
However, in current Advantest model, there is the linear/log/power modes.
What are the differences?

(2) from Agilent NA datasheet, it is found that sweep time will change with calibration
condition. E.g., un-cal, least time, 2 port cal. normal time, 4 port cal. long time.
However, as for the advantest model, it is confirmed that there is no much differences
between the calibration conditions.

Your comments are highly appreciated!

Yours,
Yiliu  

Outcomes