AnsweredAssumed Answered

Programming with COM with perl (or other scripting language)

Question asked by marcodg on Nov 25, 2011
Latest reply on Nov 27, 2011 by marcodg
Hello,  I'd like to remote control my 34410A using perl (or some other scripting language).  For most things, this would be pretty easy as I would do :

$rm = Win32::OLE->new("VisaComLib.ResourceManager");

But, for some reason this doesn't work (I took the prog-id from the VB sample; "Ivi.Visa.Interop.ResourceManager" doesn't work either).   Is this even possible?  I don't want to use .NET or other language/system that I have to compile.

(Yes I installed the drivers and the required components seem to be there; I can create this object from C#.)

Thanks,
marco  

Outcomes