AnsweredAssumed Answered

connection expert and national instrument usb

Question asked by myonezaki on Nov 21, 2011
Latest reply on Nov 21, 2011 by myonezaki
trying to use the national instrument gpib -usb-hs with the connection expert.  the usb/gpib is not shown and the device awg (33220) is not recognized.  in the past i have used agilents usb-gpib adapter which recognizes all of the test equipment on the gpib bus.  the national instrument application is installed in the computer and using its polling routine i do not see the awg(33220) on the bus but dont know if the awg's drivers are installed.  my goal is to use vba to control a awg and spectrum analyzer (e4440) connected via gpib.  many thanks  

Outcomes